AXIS#.ICONT
Description
AXIS#.ICONT returns the drive continuous rated current in Arms.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Arms |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.ICONT | 0x5000 | 0xB | DINT | 1000:1 | - | RO | False |
AXIS2.ICONT | 0x5100 | 0xB | DINT | 1000:1 | - | RO | False |